By leveraging the expertise and application knowledge of the global Schaeffler network, our Maneja and Savli plants are providing quality products for customers worldwide. A wide range of bearings manufactured in India today are supplied to customers from various segments and markets across Europe, North America and Asia Pacific regions.
From design and engineering to manufacturing and service – Schaeffler India represents the global benchmark of excellence. We have been present in India for over 50 years and Schaeffler’s three major product brands - FAG, INA and LuK - are well represented in India. With four plants and 8 sales offices, we have a significant presence in India.The two plants situated in Gujarat, in Maneja and Savli respectively are dedicated to industrial products. Schaeffler India manufactures a diversified mix of bearings for the industrial sectors at these two state-ofthe-art facilities. Both these plants follow processes that are in line with the global standard to ensure high quality world-class products for the industrial segments.
Watch the video of our India plant to find out more how Precision Bearings Made by Schaeffler – India Plant are being made.
Precision Bearings Made by Schaeffler – India Plant Video to show that quality of the bearings wherever country it is made in. Precision Bearings Made by Schaeffler – India Plant
Global Excellence, Engineered in India
By leveraging the expertise and application knowledge of the global Schaeffler network, our Maneja and Savli plants are providing quality products for customers worldwide. A wide range of bearings manufactured in India today are supplied to customers from various segments and markets across Europe, North America and Asia Pacific regions.
Maneja Plant
Our key Maneja facility was established in 1962, in Gujarat, western region of India and was renamed to 'Schaeffler India Limited' on 7 July, 2017. Spread across an estimated 99,000 m², this plant has a built up area of 36,000 m² consisting of production and service areas. Product range: Deep Groove Ball Bearings, Cylindrical Roller Bearings, Spherical Roller Bearings, Tapered Roller Bearings & TAROL Bearings. QMS Certifications: ISO 9001:2015, IATF 16949 (First Edition 2016-10-01); IRIS Certification rules: 2017; AAR M1003, AAR M934 and based on ISO/TS 22163:2017; Quality Assurance Program by Association of American Railroads) EnEHS Certification: ISO 14001: 2015, ISO 50001:2011: ISO 18001:2007
Savli Plant
Our Savli unit, also located in Gujarat, began operations in 2012, occupying 130,000 m², with a built up area of 25,000 m². This plant also carries out in-house quality related work, such as heat treatment, precision grinding and honing, with high-tech automated assembly production lines. Product range: Generation C Deep Groove Ball Bearings and Large Size Bearings Certifications: ISO 9001:2015, IATF 16949 (First Edition 2016- 10-01); ISO 14001:2015 (Environment Management System); ISO 45001:2018 (occupational health and safety (OH&S) management system); ISO 50001:2011 (Energy Management System); EMAS - III (Eco Management Auditing System)