Load carrying capacity and rating life
Permissible radial loads
The thick-walled outer rings of the track rollers can support high radial loads. If these track rollers are used against a shaft as a raceway, the outer rings undergo elastic deformation, ➤ Figure.
Compared to rolling bearings supported in a housing bore, track rollers have the following characteristics:
- modified load distribution in the bearing. This is taken into consideration by means of the basic load ratings Cr w and C0r w used in the calculation of the rating life
- bending stress in the outer ring. This is taken into consideration by means of the permissible radial loads Fr per and F0r per. The bending stresses must not exceed the permissible strength values of the material (due to the risk of fracture).
Permissible radial load under dynamic loading
For rotating bearings under dynamic load, the effective dynamic load rating Cr w is used. Cr w is used to calculate the basic rating life.
ACHTUNG
The permissible dynamic radial load Fr per must not be exceeded.
If the basic static load rating C0r w is lower than the basic dynamic load rating Cr w, C0r w is used.
Deformation of the outer ring when used against a flat raceway

Permissible radial load under static loading
For bearings under static load, when stationary or with only infrequent motion, the effective static load rating C0r w is used. C0r w is used to calculate the static load safety factor S0.
ACHTUNG
At the same time, the permissible static radial load F0r per must not be exceeded.
In addition to the permissible radial load of the bearing, the permissible radial load of the mating track must also be taken into consideration.
The basic load ratings stated are valid only in conjunction with a shaft as a mating track that is hardened (at least 670 HV) and ground (Ra 0,3).
Fatigue limit load
The fatigue limit load Cur w is defined as the load below which – under laboratory conditions – no fatigue occurs in the material.
Calculation of the rating life
The general methods for calculating the rating life are:
- the basic rating life in accordance with DIN ISO 281
- the adjusted rating life in accordance with DIN ISO 281
- the expanded calculation of the adjusted reference rating life in accordance with DIN ISO 281-4.
These methods are described in Catalogue HR 1, Rolling Bearings, in the chapter Load carrying capacity and rating life.
Rating life of track rollers
In comparison with Catalogue HR 1, Rolling Bearings, the following values must be exchanged:
Cr | = | Crw | |
C0r | = | C0r w | |
Cur | = | Cur w. |
The carriages LFCL, LFL..-SF, LFLL, LFKL..-SF and bogie carriage LFDL contain four track rollers LFR.
The equivalent principle applies here. The corresponding parameters are taken into consideration in the basic load ratings Cy, C0y, Cz, C0z and the permissible moment ratings M0x, M0y and M0z.
Cy | N | Basic dynamic load rating in y direction |
C0y | N | Basic static load rating in y direction |
Cz | N | Basic dynamic load rating in z direction |
C0z | N | Basic static load rating in z direction |
M0x | Nm | Static moment rating about x axis |
M0y | Nm | Static moment rating about y axis |
M0z | Nm | Static moment rating about z axis. |
In the case of track rollers with a profiled outer ring, calculation is carried out exclusively by means of the basic rating life to DIN ISO 281.
Load carrying capacity and load directions

Other formulae for calculating the basic rating life



Rating life for carriages with four track rollers



Ls | 105 m | Basic rating life in metres |
Da | mm | Rolling contact diameter of track roller |
Cr w, Cy, Cz | N | Effective dynamic load rating |
Pr | N | Equivalent dynamic load (radial load) |
p | Ball: p = 3; | |
Lh | h | Basic rating life in operating hours |
H | m | Single stroke length for reciprocating motion |
nosc | min–1 | Number of return strokes per minute |
![]() | m/min | Mean travel velocity |
P | N. | Equivalent dynamic load in the corresponding load direction (for applications with combined loads, please contact us). |
Operating life
The operating life is the life actually achieved by a rolling bearing. It may differ significantly from the calculated rating life.
This may be due to wear or fatigue as a result of:
- deviations in the operating data
- insufficient or excessive operating clearance (track roller, guideway)
- contamination
- inadequate lubrication
- operating temperature too high or too low
- reciprocating motion with very small stroke length, which can lead to false brinelling
- high vibration load, leading to false brinelling
- very high shock loads (static overloading)
- prior damage during mounting.
Due to the variety of mounting and operating conditions, the operating life cannot be precisely calculated in advance. The most reliable way of arriving at a close estimate is by comparison with similar applications.
Static load safety factor
The indicator of static loading is the static load safety factor S0.
This indicates the security against impermissible permanent deformations in the bearing and is determined by means of the following equation:
Static load safety factor for carriages with four track rollers


S0 | Static load safety factor | |
C0r w | N | Effective static load rating of track roller |
F0r | N | Static force acting in radial direction |
C0 | N | Basic static load rating of carriage |
F0 | N | Static force acting in y and z direction |
M0 | Nm | Permissible static moment in x, y, z direction |
M | Nm | Moment acting in load direction (Mx, My, Mz). |
Track rollers are regarded as heavily loaded at a static load safety factor of S0 < 4.
For applications with normal operating conditions, a value S0 > 4 is required.
When using individual track rollers, for example in conjunction with guideways, the decisive factor where required is the permissible load of the guideway.
ACHTUNG
Static load safety factors S0 < 1 cause plastic deformation of the rolling elements and the raceway, which can impair smooth running. This is only permissible for bearings with small rotary motions or in secondary applications.
Minimum load
In order to ensure that the outer ring is driven, that no slippage occurs and that the track roller does not lift from the mating track, the track rollers must be subjected to a minimum load in dynamic operation.
ACHTUNG
In general, the minimum load is calculated using the ratio C0r w/Fr < 60.
Differences
in raceway hardness
If shafts with a lower surface hardness are used (such as X46, X90), a hardness factor must be applied, see ➤ equations and ➤ Figure.


CH | N | Effective dynamic load rating |
fH | Dynamic hardness factor | |
C | N | Basic dynamic load rating |
C0H | N | Effective static load rating |
fH0 | Static hardness factor | |
C0 | N | Basic static load rating. |
Static and dynamic hardness factors for lower hardness of raceways