Crossed roller bearings
Crossed roller bearings SX :
- are suitable, due to their high running accuracy, as bearings for high precision applications (such as those in robots, machine tools, handling systems, precision mechanical and medical devices, vehicle components)
- correspond in their main dimensions to the ISO dimension series 18 with very small section height
- can support axial forces in both directions, radial loads, tilting moments and any combination of loads ➤ section
- usually allow designs with two bearing positions to be replaced by one bearing position ➤ Figure
- are very rigid (they can be supplied with normal clearance, clearance‑free or preloaded)
- are suitable for supported and suspended loads
- are always a good choice for a technically and economically leading bearing solution if compact and easy-to-fit rolling bearings with high tilting moment carrying capacity and rigidity, with uniform running free from stick-slip, low rotational resistance as well as high axial and radial runout accuracy are required in only one bearing position.
- the size of the bearing
- the design of the bearing environment
- the lubricant feeds
- the operating conditions.
- the operating conditions
- the environmental influences such as contamination, water, etc.
- the type of bearings.
- moisture and contaminants from entering the bearing
- the egress of lubricant from the bearing.
- the dimensional stability of the bearing rings and cylindrical rollers
- the material of the plastic spacers
- the lubricant
- the seal material in the adjacent construction.
- with normal clearance (radial and axial clearance)
- with low clearance (radial clearance/preload)
- with preload VSP (preload min. and max.).
- the equivalent static bearing load F0q
- the equivalent static tilting moment load M0q .
- Calculate the parameter for the load eccentricity ε according to ➤ Equation
- Determine the static radial load factor f0r . In this case:
- determine the ratio F0r/F0a in ➤ Figure or ➤ Figure respectively
- based on the ratio F0r/F0a and ε, determine the static radial load factor f0r from ➤ Figure or ➤ Figure respectively
- Determine the application factor fA ➤ Table and, where necessary, the safety factor fS
- Calculate the equivalent axial bearing load F0q and the equivalent tilting moment load M0q using the equations ➤ Equation and ➤ Equation
- Using the values for F0q and M0q, determine the load point in the static limiting load diagram for the raceway.
- with a load arrangement according to ➤ Figure
- if all the requirements are fulfilled in relation to location (the bearing rings must be rigid or firmly connected to the adjacent construction), mounting, lubrication and sealing
- if the load and speed can be regarded as constant during operation. If the load and speed are not constant, equivalent operating values can be determined that will result in the same fatigue conditions as the actual loads
- if the load ratio is Fr/Fa ≦ 8.
- Determine the ratio of the radial dynamic bearing load Fr to the axial dynamic bearing load Fa (Fr/Fa)
- Calculate the load eccentricity parameter ε ➤ Equation
- Using the values for ε and the ratio Fr/Fa, determine the dynamic load factor kF ➤ Figure
- Calculate the equivalent dynamic axial bearing load Pa = kF · Fa ➤ Equation
- Enter the equivalent dynamic axial bearing load Pa and the basic dynamic axial load rating Ca in the rating life equations L or Lh respectively and calculate the rating life ➤ Equation and ➤ Equation
- If swivel operation is present, enter the operating speed n determined in the rating life equation Lh ➤ Equation.
- Pr = Fr
- the basic dynamic radial load rating Cr .
- the criteria according to ➤ link
- the screws are tightened as specified using a torque wrench
- screw tightening factor αA = 1,6
- tightening torques ➤ Table to ➤ Table
- the permissible contact pressure is not exceeded
- screws of the recommended size, quantity and grade are used.
- the curves in the static limiting load diagrams for fixing screws in the product tables
- the maximum permissible radial load Fr per (friction locking).
- grade 8.8 (F0q · 1,65, M0q · 1,65)
- grade 12.9 (F0q · 0,8, M0q · 0,8).
- multiply the radial bearing load by an application factor fA ➤ Table
- compare the values determined with the maximum permissible radial load Fr per .
-
grade 8.8 (factor 1,8),
grade 10.9 (factor 1,6),
grade 12.9 (factor 1,5). - Insert or press the bearing
- Position the external clamping ring
- Insert the fixing screws
- tighten the screws in a crosswise sequence in order to prevent unacceptable fluctuations in the screw tensioning forces
- tightening torques MA for fixing screws➤ Table
- Insert the bearing
- Position the internal clamping ring
- Insert the fixing screws
- tighten the screws in a crosswise sequence in order to prevent unacceptable fluctuations in the screw tensioning forces.
- inaccuracies in the adjacent construction
- braced bearings due to incorrectly tightened clamping rings, fixing screws or locknuts.
- the rolling resistance of the rolling elements
- the internal clearance or bearing preload
- the friction of the spacers
- the friction of the seals
- the grease
- a deformed or defective adjacent construction
- errors during mounting.
- The bearing is lubricated using an unsuitable grease
- There is too much lubricant in the bearing
- The bearing load is too high
- The bearing is mounted unevenly
- The adjacent construction deviates from the specifications.
- Determining the bearing size
- Rigidity
- Friction and increases in temperature
- Speeds
- Bearing data
- Lubrication
- Sealing
- Design of bearing arrangements
- Mounting and dismounting.
For an overview of other product-specific features, see the Matrix for bearing preselection.
Comparison: bearing arrangement with two bearing positions/ bearing arrangement with a crossed roller bearing SX

Bearing design
Crossed roller bearings SX are compact locating bearings with high axial rigidity
Crossed roller bearings SX are bearings for high precision applications, whose main dimensions correspond to the ISO dimension series 18 with very small section height in accordance with DIN 616. They comprise outer rings, inner rings, rolling elements and plastic spacers. The outer ring is split in the circumferential direction and is held together by three sheet metal retaining rings ➤ Figure. The cylindrical rollers correspond to DIN 5402 and are in an X arrangement with each other on the raceways. The bearings are very rigid, have high running accuracy and are supplied with normal clearance, low clearance or preload. Bearings with preload have the suffix VSP, while bearings with low clearance have the suffix RL0 ➤ Table. The bearing outer rings are easily fixed to the adjacent construction using clamping rings ➤ link.
Also available in a corrosion-resistant design
For applications requiring high corrosion protection, the bearings are also available in a corrosion-resistant design with the special coating Corrotect.
Crossed roller bearing SX

Permissible circumferential velocities
Influencing factors
The possible circumferential velocity is dependent on the bearing (normal clearance or preloaded) and on the lubrication (grease or oil) ➤ Table.
Permissible circumferential velocities
Normal clearance |
Preload |
Circumferential velocity |
---|---|---|
Oil lubrication |
‒ |
up to 8 m/s (n · DM = 152 800) |
Grease lubrication |
‒ |
up to 4 m/s (n · DM = 76 400) |
‒ |
Oil lubrication |
up to 4 m/s (n · DM = 76 400) |
‒ |
Grease lubrication |
up to 2 m/s (n · DM = 38 200) |
DM = rolling element pitch circle diameter
Load carrying capacity
Suitable for axial loads in both directions, radial loads and tilting moment loads
Due to the X arrangement of the cylindrical rollers, the bearings can support axial forces in both directions, radial loads, tilting moment loads and any combination of loads by means of a single bearing position ➤ Figure. As a result, it is generally possible to reduce conventional bearing arrangements comprising two bearing positions (bearing arrangement with one radial and one axial bearing) to one bearing position ➤ Figure and ➤ Figure. This reduces the work required and the costs for the design of the adjacent construction (only one bearing position is processed) and considerably reduces the mounting of the bearings (there is no requirement for the matching of two bearings to each other).
Conventional bearing arrangement with two bearing positions

Optimised bearing arrangement with one crossed roller bearing

Angular adjustment facility
Crossed roller bearings SX cannot be used for the compensation of misalignments. These bearings are precision bearings for high precision applications. In order to ensure their correct function, it is essential that the specifications for design of the adjacent construction are observed ➤ section. Skewing of the bearing rings increases the running noise, places increased strain on the plastic spacers, has a negative effect on the running accuracy and a highly detrimental influence on the operating life of the bearings.
Lubrication
Grease or oil lubrication is possible
The bearings are greased as standard but can alternatively be lubricated with oil. The decisive factors in determining the type of lubrication and the requisite lubricant quantity are:
If there is any uncertainty as to whether the lubricant or type of lubrication is suitable for a particular application, please consult Schaeffler or the lubricant manufacturer respectively.
Grease lubrication
Suitable greases
If the bearing is to be lubricated with grease, a high quality lithium soap grease to DIN 51825–KP2N–20 is suitable, for example Arcanol Load150 or Load220.
Lubrication intervals
Influences on the lubrication interval
The lubrication intervals are essentially dependent on:
Precise lubrication intervals can only be determined by means of tests under the specific application conditions. The observation period selected must be sufficiently long and the condition of the grease must be checked at regular intervals.
Grease operating life
If relubrication is not possible, the grease operating life becomes the decisive factor. Based on experience, the guide value for the grease operating life in the majority of applications is higher by a factor of 2 than the guide value for the lubrication interval. At operating temperatures above +70 °C, the lubrication interval and therefore the grease operating life are reduced. In order to ensure operational reliability, the grease operating life should not exceed 3 years.
Oil lubrication
Selection of the oil
A lubricant film which is capable of supporting loads must form in the contact zones between the rolling elements and the raceway. Depending on the operating speed, the oil at operating temperature must have at least the nominal viscosity ν 1 . The guide value for ν 1 is dependent on the mean bearing diameter dM and the speed.
Influence of temperature on viscosity
As the temperature increases, the viscosity of the oil decreases. When selecting the viscosity, the lower operating temperature must also be taken into consideration. With increasing viscosity, the flowability of the lubricant is reduced. As a result, the level of power losses will increase.
Suitable oils
For oil lubrication, suitable oils are type CLP to DIN 1517 or HLP to DIN 51524 of the viscosity classes ISO VG 10 to 100.
With oil lubrication, oil change intervals must be observed
At higher temperatures, aged oil and additives in the oil can impair the operating life of the plastic used for the spacers. Stipulated oil change intervals must therefore be observed.
Sealing
Provide seals in the adjacent construction
Crossed roller bearings SX are not sealed. As a result, sealing of the bearing position must be carried out in the adjacent construction. This must reliably prevent:
Schaeffler seal profiles
Material by the metre for radial and/or axial sealing of the bearing position
For sealing of the bearing position in the adjacent construction, Schaeffler supplies various seal profiles by the metre ➤ Figure. These profiles are intended for axial and/or radial sealing and – depending on the seal profile – fulfil a wide range of requirements (for example: under normal requirements for sealing, under heavy contamination, for low frictional torque, if only limited space is available, for sealing of fluids, at low speeds or under swivel operation). In addition to the seal profiles with a radial or axial sealing effect respectively, double direction profiles (with both axial and radial sealing effect) are also available. Mounting drawings can be requested for the individual seal profiles.
The seal profiles are not suitable for applications that require leakage-free operation; this applies not only to oil but also to grease lubrication. If leakage losses are unacceptable, measures such as rotary shaft seals can be used. The area around the bearing seal must be designed such that the seal profiles are not damaged during operation.
Seal profiles – example

Seal profile material
The standard material for the profiles is the synthetic elastomer NBR 70. This material has good resistance to oil and grease as well as good wear resistance. Operating temperature of seal profiles ➤ Table.
For further information on the seal profiles, please contact Schaeffler.
Speeds
Limiting speeds in the product tables
Rolling bearings cannot rotate at unspecified high speeds, but are generally restricted by the operating temperature that is permissible in relation to the lubricant and the material of the bearing parts ➤ section. The product tables give the kinematic limiting speeds nG oil and nG grease for the bearings.
The limiting speeds nG oil and nG grease are the kinematically permissible speeds for a bearing and apply to oil and grease lubrication respectively. Even under favourable mounting and operating conditions, these speeds must not be exceeded without prior consultation with Schaeffler.
Noise
Schaeffler Noise Index
The Schaeffler Noise Index (SGI) is not yet available for this bearing type. The data for these bearing series will be introduced and updated in stages.
Temperature range
Limiting values
The operating temperature of the bearings is limited by:
Possible operating temperatures of the bearings ➤ Table.
Permissible temperature ranges
Operating temperature |
Crossed roller bearings |
Schaeffler seal profiles |
---|---|---|
|
–30 °C to +100 °C |
–40 °C to +80 °C |
In the event of anticipated temperatures which lie outside the stated values, please contact Schaeffler.
Cages
The rollers are guided by plastic spacers
In the crossed roller bearings SX, the rolling elements are separated from each other and guided not by typical rolling bearing cages but by plastic spacers ➤ Figure. The plastic selected and the design of the running surfaces for the cylindrical rollers give low-friction running of the bearings.
Internal clearance
The crossed roller bearings are available:
Dimensions, tolerances
The dimensions of special bearings (F../Z..) may deviate from the standard.
Dimension standards
The main dimensions of crossed roller bearings correspond to dimension series 18 in accordance with DIN 616.
Tolerances
The dimensional and running tolerances are based on DIN 620-2 and DIN 620-3 and are in the range P6 and P5.
Suffixes
Suffixes describe the design and features of a bearing in more detail.
Suffixes and corresponding descriptions
Suffix |
Description of suffix |
|
---|---|---|
RR |
Corrosion-resistant design, |
Special design, |
RL0 |
Low clearance |
Standard |
VSP |
Preloaded |
Special design, |
VSP+PRL50 |
Preloaded, axial and radial runout tolerance restricted by 50% |
Special design, |
Structure of bearing designation
With medias interchange, equivalent Schaeffler bearing designations can be determined for bearing designations from other rolling bearing manufacturers http://www.schaeffler.de/std/1B69.
Example
The designation of bearings follows a set model ➤ Figure.
Crossed roller bearing SX, low clearance: designation structure

Dimensioning
Static load carrying capacity
For bearings under static loading, the static load carrying capacity applies
Crossed roller bearings that undergo rotary motion only infrequently, undergo slow swivel motion, rotate only slowly or are subjected to load while stationary are dimensioned on the basis of their static load carrying capacity. The size of a statically loaded bearing can therefore be checked in approximate terms using the basic static load ratings C0 and the static limiting load diagrams.
Checking the static load carrying capacity
It can be checked in approximate terms if the correct load arrangement is present and all the requirements relating to clamping rings, location, mounting and lubrication are fulfilled ➤ Figure.
Where load arrangements are more complex or there are variations from the conditions, please contact us.
Load arrangement

In order to check the static load carrying capacity, the following equivalent static operating values must be determined:
Checking is possible for applications with or without radial load.
Determining the equivalent static bearing load without radial load
In the presence of axial and tilting moment loads only ➤ Equation and ➤ Equation:Equivalent axial bearing load (static)

Equivalent tilting moment load (static)

Legend
F0q | kN |
Equivalent axial bearing load (static) |
F0a | kN |
Axial static bearing load |
fA |
Application factor ➤ Table |
|
fS |
Factor for additional safety ➤ link |
|
M0q | kNm |
Equivalent tilting moment load (static) |
M0k | kNm |
Static tilting moment load. |
The values for F0q and M0q are used to determine the load point in the static limiting load diagram for the raceway.
In addition to the raceway, the dimensioning of the fixing screws must also be checked.
The static limiting load diagrams for the raceway and the fixing screws are indicated in the product tables.
The load point must lie under the raceway curve, otherwise the bearing is not adequately dimensioned.
Determining the equivalent static bearing load with radial load
Radial loads can only be taken into consideration if the radial load F0r is smaller than the basic static radial load rating C0r .
The equivalent static bearing load with radial load is determined as follows:
The load point must lie under the raceway curve, otherwise the bearing is not adequately dimensioned.
Load eccentricity parameter

Equivalent bearing load (static)

Equivalent tilting moment load (static)

Legend
ε |
Load eccentricity parameter |
|
M0k | kNm |
Static tilting moment load |
F0a | kN |
Axial static bearing load |
DM | mm |
Rolling element pitch circle diameter |
F0q | kN |
Equivalent bearing load (static) |
fA |
Application factor ➤ Table |
|
fS |
Factor for additional safety ➤ link |
|
f0r | ||
M0q | kNm |
Equivalent tilting moment load (static). |
Static radial load factor

Static radial load factor

Application factors
The application factors fA are empirical values obtained in practice ➤ Table. They take account of the most important requirements, such as the type and severity of operation, rigidity and running accuracy. If the precise requirements of an application are known, the values may be altered accordingly.
Application factors < 1 must not be used.
A large proportion of applications can be statically calculated using the factor 1, for example in the case of bearings for gearboxes and rotary tables.
In addition to static calculation, the rating life should also always be checked ➤ link.
Application factors fA
Application |
Operating and |
Application factor fA |
---|---|---|
Robots |
Rigidity |
1,25 |
Antennae |
Accuracy |
1,5 |
Machine tools |
Accuracy |
1,5 |
Metrology |
Smooth running |
2 |
Medical equipment |
Smooth running |
1,5 |
Safety factors
The factor for additional safety fS is 1.
It is not normally necessary to factor in any additional safety in calculation.
In special cases, such as approval specifications, internal specifications, requirements stipulated by inspection bodies etc., the appropriate safety factors must be applied.
Calculation example
The static load carrying capacity of the crossed roller bearing SX011860 is to be checked.
Given
Static bearing load (axial) |
F0a |
= |
70 kN |
Static bearing load (radial) |
F0r |
= |
17,5 kN |
Static tilting moment load |
M0k |
= |
22,5 kNm |
Rolling element pitch circle diameter |
DM |
= |
340 mm |
Application factor |
fA |
= |
1,25 |
Safety factor |
fS |
= |
1 |
Required
Static load carrying capacity of the bearing
Solution
Load eccentricity parameter

Legend
ε |
Load eccentricity parameter |
|
M0k | kNm |
Static tilting moment load |
F0a | kN |
Static bearing load (axial) |
DM | mm |
Rolling element pitch circle diameter |
F0r | kN |
Static bearing load (radial) |
f0r |
Equivalent bearing load (static)

Legend
F0q | kN |
Equivalent bearing load (static) |
F0a | kN |
Static bearing load (axial) |
fA |
Application factor |
|
fS |
Factor for additional safety. |
Equivalent tilting moment load (static)

Legend
M0q | kNm |
Equivalent tilting moment load (static) |
M0k | kNm |
Static tilting moment load |
fA |
Application factor |
|
fS |
Factor for additional safety. |
Determining the load point in the static limiting load diagram – checking the static load carrying capacity
Using the values for F0q and M0q, the load point in the static limiting load diagrams for the raceway and fixing screws is determined ➤ Figure and ➤ Figure.
The load point is below the raceway and screw curves. The bearing is adequately dimensioned and thus suitable for the application.
Static limiting load diagram for raceway – compressive load

Static limiting load diagram for fixing screws – compressive load

Dynamic load carrying capacity
For bearings under dynamic loading, the dynamic load carrying capacity applies
Dynamically loaded crossed roller bearings, i. e. bearings that undergo predominantly rotary motion, are dimensioned in accordance with their dynamic load carrying capacity. The size of a dynamically loaded bearing can therefore be checked in approximate terms using the basic dynamic load ratings C and the basic rating life L or Lh.
Determining the basic rating life
The life formulae for L and Lh are only valid:
For more complex load arrangements, if a ratio Fr/Fa > 8 is present or there are variations from the specified conditions, please contact us.
Load arrangement

Determining the basic rating life for bearings subjected to combined loads
For bearings subjected to combined loads, in other words bearings with axial, radial and tilting moment loads, the rating life L or Lh is determined as follows:
Load eccentricity parameter

Equivalent dynamic axial bearing load

Basic rating life in millions of revolutions

Basic rating life in operating hours

Operating speed

Dynamic load factor

Determining the basic rating life for bearings subjected to radial loads only
For slewing rings subjected to radial loads only, the following values are entered in the rating life formulae L and Lh:
Basic rating life in millions of revolutions

Basic rating life in operating hours

Legend
ε |
Load eccentricity parameter |
|
Mk | kNm |
Dynamic tilting moment load |
Fa | kN |
Axial dynamic bearing load |
DM | mm |
Rolling element pitch circle diameter |
Pa | kN |
Equivalent dynamic axial bearing load. For bearings subjected to radial load only, enter Pr |
kF |
Dynamic load factor ➤ Figure |
|
L10 | 106 |
Basic rating life in millions of revolutions |
Ca, Cr | kN |
Basic axial or radial dynamic load rating. For bearings subjected to radial load only, enter Cr |
p |
Life exponent for crossed roller bearings: p = 10/3 |
|
L10h | h |
Basic rating life in operating hours |
n | min–1 |
Operating speed |
nosc | min–1 |
Frequency of oscillating motion |
γ | ° |
Half of swivel angle |
Pr | kN |
Equivalent dynamic radial bearing load |
Fr | kN |
Radial dynamic bearing load. |
Calculation example
For the crossed roller bearing SX011820, the basic rating life L in millions of revolutions is to be checked.
Given
Crossed roller bearing |
SX011820 |
||
Rolling element pitch circle diameter |
DM |
= |
112 mm |
Basic dynamic load rating (axial) |
Ca |
= |
28 kN |
Life exponent for crossed roller bearings |
p |
= |
10/3 |
Dynamic bearing load (axial) |
Fa |
= |
20 kN |
Dynamic bearing load (radial) |
Fr |
= |
4 kN |
Dynamic tilting moment load |
Mk |
= |
1 kNm |
Required
Basic rating life L10 in millions of revolutions
Solution
Load eccentricity parameter

Legend
ε |
Load eccentricity parameter |
|
Mk | kNm |
Dynamic tilting moment load |
Fa | kN |
Axial dynamic bearing load |
DM | mm |
Rolling element pitch circle diameter |
Fr | kN |
Radial dynamic bearing load |
kF |
Dynamic load factor ➤ Figure. |
Equivalent bearing load (static)

Legend
Pa | kN |
Equivalent dynamic axial bearing load. For bearings subjected to radial load only, enter Pr |
kF |
Dynamic load factor ➤ Figure |
|
Fa | kN |
Axial dynamic bearing load. |
Basic rating life in million revolutions

Legend
L10 | 106 |
Basic rating life in millions of revolutions For bearings subjected to radial load only, enter Pr |
Ca, Cr | kN |
Basic axial or radial dynamic load rating |
Pa | kN |
Equivalent dynamic axial bearing load. For bearings subjected to radial load only, enter Pr |
p |
Life exponent for crossed roller bearings: p = 10/3. |
Dynamic load factor kF for crossed roller bearings

Determining the load carrying capacity of the fixing screws
In addition to the raceway, the load carrying capacity of the fixing screws must also be checked. This is based on the information in ➤ link.
The load carrying capacity of the fixing screws can be checked if the following conditions are fulfilled:
Indicator of load carrying capacity
The load carrying capacity of the screws is described by:
The screw curves are shown in the static limiting load diagrams for fixing screws. The curves are based on screws of grade 10.9, tightened to 90% of their proof stress, including the torsion content.
If screws of grade 8.8 or 12.9 are used, the equivalent static loads F0q and M0q, ➤ link, must be converted using the following factors:
Static limiting load diagram for fixing screws – example
Static limiting load diagram for fixing screws – example for crossed roller bearing SX011860

Checking the static load carrying capacity of the screws
The static load carrying capacity of the screw is limited by its proof stress.
For applications with and without radial load
The equivalent static bearing loads F0q and M0q must be determined.
Using the values F0q and M0q, the load point is then determined in the static limiting load diagram for fixing screws.
The load point must be below the appropriate screw curve.
Radial load and static load carrying capacity of the screws
If radial loads occur in uncentred bearing rings, the screw connections must prevent displacement of the bearing rings on the adjacent construction.
In order to check this:
The maximum radial load Fr per on the fixing screws is dependent on their friction locking and not on the radial load carrying capacity of the bearing.
If the radial load on the bearing is higher than the friction locking of the fixing screws or very high radial loads are present (Fr/Fa > 4), please contact us.
Checking the dynamic load carrying capacity of the screws
The dynamic load carrying capacity of the screws corresponds to the fatigue strength of the screw.
Dynamic load carrying capacity
Based on the dynamic loads present, the equivalent loads F0q and M0q are determined.
Instead of the application factor fA , the operating load must always be increased by the following factor:
The load carrying capacity must then be checked in the static limiting load diagram for the fixing screws.
The load point must be below the appropriate screw curve.
Minimum load
In order to prevent damage due to slippage, a minimum load is required
In order that no slippage occurs between the contact partners, the crossed roller bearings must be constantly subjected to a sufficiently high load. In most cases, however, the load is already sufficiently high due to the weight of the supported parts and the external forces.
Design of bearing arrangements
The design of the adjacent construction has a considerable influence on the function of the bearings
Crossed roller bearings SX can support high loads. Due to the X arrangement of the cylindrical rollers, these bearings can support axial forces in both directions, radial loads, tilting moment loads and any combinations of loads. In order that these advantages can be utilised comprehensively, the adjacent construction must be designed so that it is appropriately rigid. The bearing rings must always be rigidly and uniformly supported over the circumference and width of the rings ➤ Figure.
The adjacent construction must be designed only in accordance with the information in this section. Any deviations from the specifications, material strength and adjacent components will considerably reduce the load carrying capacity and operating life of the bearings.
Uniform support of the bearing rings by the adjacent construction

Shaft and housing tolerances
For normal applications, the tolerance class K7 Ⓔ for the housing and h7 Ⓔ for the shaft are sufficient ➤ Table and ➤ Table.
In precision applications, the bearing seat in the housing should be designed to tolerance class K6 Ⓔ and on the shaft to h6 Ⓔ ➤ Table and ➤ Table.
Mounting tolerances for the shaft
Nominal dimension di |
Tolerance classes |
||||
---|---|---|---|---|---|
mm |
|||||
> |
≦ |
h6 |
h7 |
||
Upper deviation |
Lower deviation |
Upper deviation |
Lower deviation |
||
μm |
μm |
μm |
μm |
||
65 |
80 |
0 |
–19 |
0 |
–30 |
80 |
100 |
0 |
–22 |
0 |
–35 |
100 |
120 |
0 |
–22 |
0 |
–35 |
120 |
140 |
0 |
–25 |
0 |
–40 |
140 |
160 |
0 |
–25 |
0 |
–40 |
160 |
180 |
0 |
–25 |
0 |
–40 |
continued ▼ |
Mounting tolerances for the shaft
Nominal dimension di |
Tolerance classes |
||||
---|---|---|---|---|---|
mm |
|||||
> |
≦ |
h6 |
h7 |
||
Upper deviation |
Lower deviation |
Upper deviation |
Lower deviation |
||
μm |
μm |
μm |
μm |
||
180 |
200 |
0 |
–29 |
0 |
–46 |
200 |
225 |
0 |
–29 |
0 |
–46 |
225 |
250 |
0 |
–29 |
0 |
–46 |
250 |
280 |
0 |
–32 |
0 |
–52 |
280 |
315 |
0 |
–32 |
0 |
–52 |
315 |
355 |
0 |
–36 |
0 |
–57 |
355 |
400 |
0 |
–36 |
0 |
–57 |
400 |
450 |
0 |
–40 |
0 |
–63 |
450 |
500 |
0 |
–40 |
0 |
–63 |
continued ▲ |
Mounting tolerances for the housing bore
Nominal dimension Da |
Tolerance classes |
||||
---|---|---|---|---|---|
mm |
|||||
> |
≦ |
K6 |
K7 |
||
Upper deviation |
Lower deviation |
Upper deviation |
Lower deviation |
||
μm |
μm |
μm |
μm |
||
80 |
100 |
+4 |
–18 |
+10 |
–25 |
100 |
120 |
+4 |
–18 |
+10 |
–25 |
120 |
140 |
+4 |
–21 |
+12 |
–28 |
140 |
160 |
+4 |
–21 |
+12 |
–28 |
160 |
180 |
+4 |
–21 |
+12 |
–28 |
180 |
200 |
+5 |
–24 |
+13 |
–33 |
200 |
225 |
+5 |
–24 |
+13 |
–33 |
225 |
250 |
+5 |
–24 |
+13 |
–33 |
250 |
280 |
+5 |
–27 |
+16 |
–36 |
280 |
315 |
+5 |
–27 |
+16 |
–36 |
315 |
355 |
+7 |
–29 |
+17 |
–40 |
355 |
400 |
+7 |
–29 |
+17 |
–40 |
400 |
450 |
+8 |
–32 |
+18 |
–45 |
450 |
500 |
+8 |
–32 |
+18 |
–45 |
500 |
560 |
0 |
–44 |
0 |
–70 |
560 |
630 |
0 |
–44 |
0 |
–70 |
Location using clamping rings
For the location of crossed roller bearings SX, clamping rings have proved effective ➤ Figure.
The bearing rings must always be rigidly and uniformly supported over the circumference and width of the rings.
The thickness of the clamping rings and mounting flanges must not be less than the minimum thickness s.
Counterbores to DIN 74, type J, for screws to DIN 6912 are permissible. For deeper counterbores, the thickness of the clamping ring s must be increased by the additional counterbore depth.
Mounting dimensions ➤ Table and ➤ Figure . Minimum strength of clamping rings ➤ link .
Bearing seat depth
In order that the clamping rings retain the bearing securely, the bearing seat depth t must be in accordance with the specification ➤ Table and ➤ Figure.
The depth of the bearing seat influences the bearing clearance and the rotational resistance.
Bearings with preload (suffix VSP) have a considerably higher rotational resistance.
If particular requirements for rotational resistance apply, the depth t must be produced to match the relevant height of the bearing ring. It has proved effective to tolerance the depth t to deviations that are the same as or further restricted compared to the dimension h in the product tables. For safety, internal tests should in any case be carried out.
Minimum strength of clamping rings
For screws of grade 10.9, the minimum strength under the screw heads or nuts must be 500 N/mm2 . Seating washers are not necessary for these screws.
For fixing screws of grade 12.9, the minimum strength must not be less than 850 N/mm2 , otherwise quenched and tempered seating washers under the screw heads or quenched and tempered nuts must be used.
Mounting dimensions
Designation |
Mounting dimensions in mm |
||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|
di |
Da |
t |
s |
dRa |
dRi |
DRi |
DRa |
Li |
La |
||
h7 (h6) |
K7 (K6) |
min. |
max. |
min. |
|||||||
SX011814 |
70 |
90 |
10 |
–0,005 –0,015 |
8 |
78 |
42 |
82 |
118 |
60 |
100 |
SX011818 |
90 |
115 |
13 |
–0,005 –0,020 |
10 |
100 |
61 |
104 |
144 |
80 |
125 |
SX011820 |
100 |
125 |
13 |
–0,005 –0,020 |
10 |
110 |
71 |
114 |
154 |
90 |
135 |
SX011824 |
120 |
150 |
16 |
–0,005 –0,025 |
12 |
132 |
84 |
138 |
186 |
108 |
162 |
SX011828 |
140 |
175 |
18 |
–0,005 –0,030 |
14 |
154 |
94 |
160 |
221 |
124 |
191 |
SX011832 |
160 |
200 |
20 |
–0,02 –0,05 |
15 |
177 |
111 |
183 |
249 |
144 |
216 |
SX011836 |
180 |
225 |
22 |
–0,02 –0,05 |
17 |
199 |
121 |
205 |
284 |
160 |
245 |
SX011840 |
200 |
250 |
24 |
–0,02 –0,06 |
18 |
221 |
139 |
229 |
311 |
180 |
270 |
SX011848 |
240 |
300 |
28 |
–0,02 –0,06 |
21 |
269 |
166 |
274 |
374 |
216 |
324 |
SX011860 |
300 |
380 |
38 |
–0,04 –0,10 |
29 |
335 |
201 |
345 |
479 |
268 |
412 |
SX011868 |
340 |
420 |
38 |
–0,04 –0,10 |
29 |
375 |
241 |
385 |
519 |
308 |
452 |
SX011880 |
400 |
500 |
46 |
–0,04 –0,10 |
35 |
445 |
275 |
455 |
625 |
360 |
540 |
SX0118/500 |
500 |
620 |
56 |
–0,04 –0,10 |
42 |
554 |
350 |
566 |
700 |
452 |
668 |
Clamping rings, bearing seat depth, mounting dimensions

Fixing screws
For the location of the bearing rings or clamping rings, screws of grade 10.9 are suitable ➤ Table.
Any deviations from the recommended size, grade and quantity of screws will considerably reduce the load carrying capacity and operating life of the bearings.
For screws of grade 12.9, the minimum strength of the clamping rings must be achieved or quenched and tempered seating washers must be used.
Fixing screws
Crossed roller bearings |
Fixing screws Grade 10.9 |
Tightening torque |
|
---|---|---|---|
Dimension |
Quantity |
MA Nm |
|
SX011814 |
M5 |
18 |
7 |
SX011818 |
M5 |
24 |
7 |
SX011820 |
M5 |
24 |
7 |
SX011824 |
M6 |
24 |
11,7 |
SX011828 |
M8 |
24 |
27,8 |
SX011832 |
M8 |
24 |
27,8 |
SX011836 |
M10 |
24 |
55,6 |
SX011840 |
M10 |
24 |
55,6 |
SX011848 |
M12 |
24 |
98,4 |
SX011860 |
M16 |
24 |
247 |
SX011868 |
M16 |
24 |
247 |
SX011880 |
M20 |
24 |
481 |
SX0118/500 |
M24 |
24 |
831 |
Securing of screws
Normally, the screws are adequately secured by the correct preload ➤ Table and ➤ Table. If regular shock loads or vibrations occur, however, additional securing of the screws may be necessary.
Not every method of securing screws is suitable for crossed roller bearings. Never use spring washers or split washers.
General information on securing of screws is given in DIN 25201-4:2004. If these are to be used, please consult the relevant companies.
Tightening torques MA for the torque-controlled tightening of socket headless screws
Fixing screw |
Clamping cross‑section |
Core cross‑section |
Tightening torque MA ** in Nm for grade |
||
---|---|---|---|---|---|
AS |
Ad3 |
8.8 |
10.9 |
12.9 |
|
mm2 |
mm2 |
||||
M4 |
8,78 |
7,75 |
2,25 |
3,31 |
3,87 |
M5 |
14,2 |
12,7 |
4,61 |
6,77 |
7,92 |
M6 |
20,1 |
17,9 |
7,8 |
11,5 |
13,4 |
M8 |
36,6 |
32,8 |
19,1 |
28 |
32,8 |
M10 |
58 |
52,3 |
38 |
55,8 |
65,3 |
M12 |
84,3 |
76,2 |
66,5 |
97,7 |
114 |
M14 |
115 |
105 |
107 |
156 |
183 |
M16 |
157 |
144 |
168 |
246 |
288 |
M18 |
192 |
175 |
229 |
336 |
394 |
M20 |
245 |
225 |
327 |
481 |
562 |
M22 |
303 |
282 |
450 |
661 |
773 |
M24 |
353 |
324 |
565 |
830 |
972 |
** MA in accordance with guideline VDI 2230 (February 2003) for μK = 0,08 and μG = 0,12.
Assembly preload forces FM for the torque-controlled tightening of socket headless screws
Fixing screw |
Clamping cross‑section |
Core cross‑section |
Mounting preload force FM ** in kN for grade |
||
---|---|---|---|---|---|
AS |
Ad3 |
8.8 |
10.9 |
12.9 |
|
mm2 |
mm2 |
||||
M4 |
8,78 |
7,75 |
4,05 |
5,95 |
6,96 |
M5 |
14,2 |
12,7 |
6,63 |
9,74 |
11,4 |
M6 |
20,1 |
17,9 |
9,36 |
13,7 |
16,1 |
M8 |
36,6 |
32,8 |
17,2 |
25,2 |
29,5 |
M10 |
58 |
52,3 |
27,3 |
40,2 |
47 |
M12 |
84,3 |
76,2 |
39,9 |
58,5 |
68,5 |
M14 |
115 |
105 |
54,7 |
80,4 |
94,1 |
M16 |
157 |
144 |
75,3 |
111 |
129 |
M18 |
192 |
175 |
91,6 |
134 |
157 |
M20 |
245 |
225 |
118 |
173 |
202 |
M22 |
303 |
282 |
147 |
216 |
253 |
M24 |
353 |
324 |
169 |
249 |
291 |
** FM in accordance with guideline VDI 2230 (February 2003) for μG = 0,12.
Mounting and dismounting
Mounting of crossed roller bearings
The bores and edges of the adjacent components must be free from burrs. The support surfaces for the bearing rings must be clean.
The seating and locating surfaces for the bearing rings on the adjacent construction must be lightly oiled or greased.
Lightly oil the thread of the fixing screws in order to prevent varying friction factors (do not oil or grease screws that will be secured by means of adhesive).
Ensure that all adjacent components and lubrication ducts are free from cleaning agents, solvents and washing emulsions. The bearing seat surfaces can rust or the raceway system can become contaminated.
Mounting forces must only be applied to the bearing ring to be mounted; forces must never be directed through the rolling elements or seals. Avoid direct blows on the bearing rings in all cases.
Locate the bearing rings consecutively and without application of any external load.
The outer ring is split and is held together by three retaining rings

Locating the outer bearing ring
Mounting of the ring ➤ Figure:
Locating the outer bearing ring

Locating the inner bearing ring
Mounting of the ring ➤ Figure :
Locating the inner bearing ring

Checking the function
Once mounting is complete, the operation of the mounted crossed roller bearing must be checked. If the bearing runs irregularly or roughly, or the temperature in the bearing shows an unusual increase, the bearing must be dismounted, checked and mounted again in accordance with the mounting guidelines described.
Checking the running accuracy
Possible causes of deviations in values
The running accuracy must be checked by means of a dial gauge. The corresponding values are taken from the mounting drawing or the product tables. Deviations from the values may be the result of:
Checking the rotational resistance
Factors influencing the rotational resistance
The rotational resistance is essentially determined by:
Preload, rotational resistance, bearing temperature
Due to the preload in the rolling element system, the rotational resistance is higher than in a bearing with clearance. At higher speeds, a high preload can lead to generation of significant heat in the bearing. In such applications, tests must be carried out if necessary with bearings preloaded to various values.
Checking the bearing temperature
Possible causes of high temperatures
After commissioning, the temperature in the bearing can increase; in the case of grease lubrication, this may continue until the grease is evenly distributed in the bearing. A further increase or unusually high temperatures may be caused by one of the following:
Schaeffler Mounting Handbook
Rolling bearings must be handled with great care
Rolling bearings are well-proven precision machine elements for the design of economical and reliable bearing arrangements, which offer high operational security. In order that these products can function correctly and achieve the envisaged operating life without detrimental effect, they must be handled with care.
The Schaeffler Mounting Handbook MH 1 gives comprehensive information about the correct storage, mounting, dismounting and maintenance of rotary rolling bearings http://www.schaeffler.de/std/1D53. It also provides information which should be observed by the designer, in relation to the mounting, dismounting and maintenance of bearings, in the original design of the bearing position. This book is available from Schaeffler on request.
Further information
In addition to the data in this chapter, the following chapters in Technical principles must also be observed in the design of bearing arrangements: