Load carrying capacity and rating life

Load carrying capacity and rating life

Dimensioning of driven linear units

The performance capacity of a driven linear unit is essentially determined by the bearings, guidance systems and drive elements used.

The required size of these elements is dependent on the following requirements:

  • rating life
    • load carrying capacity
      • operational reliability.

        As a result of the complex interaction of the bearings, guidance systems and drive elements, it is advisable in practice to use manual calculation for preselection only. Precise calculation should be carried out using software from the BEARINX range.

        Monorail guidance systems in driven linear units

        The size of a monorail guidance system is determined by the demands made on its load carrying capacity, rating life and operational reliability.

        Load carrying capacity

        The load carrying capacity is described in terms of the basic dynamic load rating C, the basic static load rating C0 and the static moment ratings M0x, M0y and M0z, ➤ Figure.

        The basic dynamic load rating is the load in N at which the guidance system achieves a distance of 100 km at a survival probability of 90% (C100).

        Load carrying capacity and load direction
        Calculation of basic load ratings according to DIN

        The calculation of the basic dynamic and static load ratings for each carriage in the dimension tables is based on DIN 636-1 and 2.

        Differences between DIN and suppliers from the Far East

        Suppliers from the Far East frequently calculate basic load ratings using a basic rating life based on a distance of only 50 km compared with 100 km to DIN.

        Linear recirculating ball bearing and guideway assemblies

        C50 N

        Basic dynamic load rating C for a distance of 50 km

        C100 N

        Basic dynamic load rating C for a distance of 100 km –
        definition according to DIN 636.

        Basic rating life

        The basic rating life L or Lh is achieved or exceeded by 90% of a sufficiently large group of apparently identical bearings before the first evidence of material fatigue occurs.

        Equivalent load and speed

        The equations for calculating the basic rating life are based on the assumption that the load P and travel velocity 

        are constant. Non‑constant operating conditions can be taken into consideration by means of equivalent operating values. These have the same effect as the loads occurring in practice.

        Equivalent dynamic load

        Where the load varies in steps, the equivalent dynamic load is calculated as follows:

        Equivalent dynamic travel velocity

        Where the travel velocity varies in steps, the equivalent dynamic travel velocity is calculated as follows:

        Combined load

        If the direction of the load acting on an element does not coincide with one of the main load directions, an approximate value for the equivalent load is calculated as follows:
        If an element is simultaneously subjected to a force F and a moment M, an approximate value for the equivalent dynamic load is calculated as follows:
        Symbols, units and definitions
        C N

        Basic static load rating in the direction of the force acting on the element

        C0 N

        Basic static load rating in the direction of the force acting on the element

        F N

        Force acting on the element

        Fy N

        Vertical component

        Fz N

        Horizontal component

        H m

        Single stroke length for reciprocating motion

        L, Lh km,  h

        Basic rating life in 100 km or in operating hours

        M Nm

        Moment acting on the element

        M0 Nm

        Static moment rating

        nosc min–1

        Number of return strokes per minute

        P N

        Equivalent dynamic load

        p

        Life exponent:
        monorail guidance systems based on balls = 3

        qz %

        Duration as a proportion of the total operating time

        vz m/min

        Variable travel velocity

         m/min

        Equivalent dynamic travel velocity.

        Operating life

        The operating life is the life actually achieved by a rolling bearing or a monorail guidance system. It may differ significantly from the calculated life.

        The following influences can lead to premature failure through wear or fatigue:

        • deviations in the operating data
          • excess load due to misalignment as a result of temperature differences and manufacturing tolerances in the adjacent construction (elasticity of the adjacent construction)
            • contamination of the guidance systems
              • inadequate lubrication
                • operating temperature too high or too low
                  • reciprocating motion with very small stroke length (false brinelling)
                    • vibration during stoppage (false brinelling)
                      • overloading of the guidance system, for example by shock loads (even for short periods)
                        • overloading of the linear unit (even for short periods)
                          • impermissible shaft deflection in linear tables LTE and LTS
                            • preliminary damage (plastic deformation) occurring during assembly of the adjacent construction.

                              Static load carrying capacity

                              The static load carrying capacity of the monorail guidance system incorporated in driven linear units is limited by:

                              • the permissible load on the monorail guidance system
                                • the load carrying capacity of the guideway
                                  • the mounting position
                                    • the permissible load on the screw connections
                                      • the permissible load on the adjacent construction.
                                        ATTENTION

                                        For design purposes, the static load safety factor S0 required for the application must be observed, see tables starting link.

                                        Basic static load ratings and moment ratings

                                        The basic static load ratings and static moment ratings are those loads under which the raceways and rolling elements undergo a permanent overall deformation corresponding to 1/10 000 of the rolling element diameter.

                                        Static load safety factor
                                        The static load safety factor S0 is the security against impermissible permanent deformation at the rolling contact:
                                        S0

                                        Static load safety factor

                                        C0 N

                                        Basic static load rating in the load direction

                                        P0 N

                                        Equivalent static bearing load in the load direction

                                        M0 Nm

                                        Static moment rating in the load direction (M0x, M0y, M0z)

                                        M Nm

                                        Equivalent static moment in the load direction.

                                        The equivalent static bearing load is determined in approximate terms from the maximum loads occurring:
                                        ATTENTION

                                        Static load safety factor S0 for the design of linear guidance systems, see tables.

                                        Track roller guidance systems

                                        The general methods for calculating the rating life are:

                                        • the basic rating life according to DIN ISO 281
                                          • the adjusted rating life according to DIN ISO 281
                                            • the expanded calculation of the adjusted reference rating life according to DIN ISO 281-4.

                                              These methods are described in Catalogue HR1, Rolling Bearings, in the chapter Load carrying capacity and life.

                                              Rating life of track rollers

                                              The carriages of series MLF, MLFI and MKLF are fitted with four profiled track rollers or in some sizes with three profiled track rollers.

                                              The track rollers are subject to the corresponding principle. The corresponding parameters are taken into consideration in the basic load ratings C, C0 and the permissible moment ratings M0x, M0y and M0z, ➤ Figure.

                                              CI N

                                              Basic dynamic load rating in the y (compressive) direction

                                              C0I N

                                              Basic static load rating in the y (compressive) direction

                                              CII N

                                              Basic dynamic load rating in the y (tensile) direction

                                              C0II N

                                              Basic static load rating in the y (tensile) direction

                                              CIII N

                                              Basic dynamic load rating in the z (lateral) direction

                                              C0IIIN

                                              Basic static load rating in the z (lateral) direction

                                              M0x Nm

                                              Static moment rating about the X axis

                                              M0y Nm

                                              Static moment rating about the Y axis

                                              M0z Nm

                                              Static moment rating about the Z axis.

                                              In the case of track rollers with a profiled outer ring, calculation is carried out exclusively by means of the basic rating life according to DIN ISO 281.

                                              Load carrying capacity and load directions
                                              Rating life for carriages with four track rollers
                                              Lh h

                                              Basic rating life in operating hours

                                              CI, CII, CIII N

                                              Effective dynamic load rating

                                              H m

                                              Single stroke length for reciprocating motion

                                              nosc min–1

                                              Number of return strokes per minute

                                              P N

                                              Equivalent dynamic load in the corresponding load direction (for applications with combined loads, please contact us).

                                              Static load safety factor

                                              The indicator of static loading is the static load safety factor S0. It indicates the security with regard to permissible permanent deformation of the bearing.

                                              Static load safety factor
                                              for carriages with four track rollers
                                              S0 N

                                              Static load safety factor

                                              C0 N

                                              Basic static load rating in the load direction according to the dimension table

                                              P0 N

                                              Equivalent static bearing load in the load direction

                                              M0 Nm

                                              Permissible static moment in the x, y and z direction according to the dimension table

                                              M Nm

                                              Equivalent static moment rating in the load direction (Mx, My, Mz).

                                              Minimum load safety factors for actuators with track roller guidance systems, see tables.

                                              Linear tables with linear ball bearings

                                              The size of a linear table is determined by the requirements made on its load carrying capacity, rating life and operational reliability.

                                              The load carrying capacity is described in terms of:

                                              • the basic dynamic load rating C
                                                • the basic static load rating C0.

                                                  The calculation of the basic dynamic and static load ratings in the dimension tables is based on DIN 636-1.

                                                  The carriages in linear tables with linear ball bearings are each fitted with four linear ball bearings, ➤ Figure. The calculation equations for these correspond to the equations for individual bearings. The corresponding parameters are taken into consideration in the basic load ratings of the linear tables CI, CII and CIII, or C0I, C0II and C0III, and the moment ratings M0x, M0y and M0z.

                                                  Load carrying capacity and load directions

                                                  Static load carrying capacity

                                                  The static load carrying capacity of the shaft guidance systems fitted in the linear tables LTE and LTS is restricted by:

                                                  • the permissible load on the linear ball bearings
                                                    • the permissible load on the adjacent construction
                                                      • the permissible deflection of the guidance shafts in linear tables LTE
                                                        • the load carrying capacity of the shaft and support rail units (aluminium support rail with screw mounted guidance shaft) in linear tables LTS
                                                          • the mounting position.
                                                            ATTENTION

                                                            For design purposes, the static load safety factor S0 required for the application must be observed, see tables.

                                                            Basic static load ratings and moment ratings

                                                            The basic static load ratings and static moment ratings are those loads under which the raceways and rolling elements undergo a permanent overall deformation corresponding to 1/10 000 of the rolling element diameter.

                                                            Static load safety factor
                                                            The static load safety factor S0 is the security against permanent deformation at the rolling contact:
                                                            S0

                                                            Static load safety factor

                                                            C0 N

                                                            Basic static load rating in the load direction C0I, C0II, C0III)
                                                            according to dimension tables

                                                            P0 N

                                                            Equivalent static bearing load in the load direction

                                                            M0 Nm

                                                            Basic static moment rating in the load direction (M0x, M0y, M0z)
                                                            according to dimension tables

                                                            M Nm

                                                            Equivalent static moment in the load direction.

                                                            The equivalent static bearing load is determined in approximate terms from the maximum loads occurring:
                                                            ATTENTION

                                                            Static load safety factor S0 for design of linear guidance systems, see tables starting link.

                                                            Bearing arrangement in return units for toothed belts

                                                            The bearing arrangements in the return shaft units of actuators are dimensioned such that their operating life exceeds the operating life of the guidance systems fitted in the actuator.

                                                            For this reason, checking of the load carrying capacity and rating life of the return shaft units is only necessary in exceptional cases, such as increased preload of the toothed belt and high loads on the toothed belt.

                                                            In such cases, please contact the Schaeffler engineering service.

                                                            Support bearings for ball screw drives

                                                            Actuators and linear tables with ball screw drive are fitted on the locating bearing side with double row axial angular contact ball bearings of series ZKLF..-2RS(-PE) or axial angular contact ball bearings of series ZKLN..-2RS(-PE). Linear tables with trapezoidal screw drive are fitted with single or double row angular contact ball bearings of series 30, 33 and 72.

                                                            Basic rating life of the locating bearing arrangement

                                                            The decisive factors in determining the suitability of the linear unit for the specific application are the basic rating life, the static load safety factor and the axial limiting load of the locating bearing arrangement.

                                                            The basic rating life is calculated as follows:
                                                            L 106 Umdrehungen

                                                            Basic rating life in millions of revolutions

                                                            Ca N

                                                            Dynamic axial bearing load

                                                            P N

                                                            Equivalent dynamic bearing load

                                                            Lh h

                                                            Basic rating life in operating hours

                                                            n min–1

                                                            Operating speed.

                                                            Needle roller bearings or ball bearings are used in the non-locating bearing arrangement of the screw drive. These are adequately dimensioned such that, with correct usage, their operating life exceeds the operating life of the ball screw drive.

                                                            Resultant equivalent bearing load P for ZKLN and ZKLF

                                                            The axial angular contact ball bearings of series ZKLN and ZKLF fitted in actuators and linear tables have a defined axial preload. The resultant bearing load Fa res must be determined from the axial operating load FaB taking account of the axial preload, ➤ Figure and ➤ Figure.

                                                            ATTENTION

                                                            If the load exceeds the limit values, the rolling element row without load will lift off the raceway. As a result, higher wear will occur under rapid acceleration. The calculation program BEARINX can give a precise design in this case.

                                                            Resultant bearing load ZKLN and ZKLF up to d = 17 mm
                                                             ZKLN0624 ·
                                                             ZKLN1034 ·
                                                             ZKLN1242 ·
                                                             ZKLN1545 ZKLF1560 ·
                                                             ZKLN1747 
                                                            Resultant bearing load ZKLN and ZKLF from d = 20 mm to d = 30 mm
                                                             ZKLN2052 ·
                                                             ZKLF2575 ·
                                                             ZKLF3080

                                                            Axial and radial operating loads

                                                            If the linear unit is mounted as a vertical axis, this gives an equiv­alent dynamic bearing load P = Fa res. If it is mounted horizontally, the screw drive bearing arrangement is subjected to an additional load due to the inherent mass of the spindle. For the purposes of approximate calculation, this can be disregarded.

                                                            Load varying in steps
                                                            If the load values vary in steps, the equivalent load P and speed n are calculated as follows:
                                                            q %

                                                            Time period.

                                                            Static load safety factor

                                                            The static load safety factor S0 indicates the security against impermissible permanent deformations in the bearing.

                                                            In the case of driven linear units with ball screw drive, it is calculated as follows, see ➤ equation:
                                                            S0–

                                                            Static load safety factor

                                                            C0a N

                                                            Basic static axial load rating

                                                            P0 N

                                                            Maximum static axial load of bearing.

                                                            Permissible static axial load for ZKLF

                                                            For bearings of series ZKLF fitted in driven linear units with ball screw drive, the static axial load in the direction of the screw connections is shown in ➤ Figure.

                                                            Basic static load rating C0a

                                                            Static axial load in the direction of the screw connections
                                                            ZKLF

                                                            Application-oriented static load safety factor

                                                            The static load safety factor of monorail and track roller guidance systems in actuators must not be utilised to its full extent. At all times, a minimum load safety factor S0 must be observed, see tables.

                                                            In the case of actuators and linear tables with monorail guidance system, guidance systems with high load carrying capacity and rigidity are combined with adjacent parts made from aluminium. Since these adjacent parts are made from aluminium section or aluminium plates, the static load carrying capacity of the monorail guidance systems cannot be used to its full extent since this is only partially permitted by the screw connections.

                                                            Furthermore, geometrical inaccuracies of the aluminium parts, alignment defects in multi-axis arrangements and deformations due to load in mounting with unsupported lengths must be taken into consideration. Since it is difficult to specify these influences, minimum load safety factors determined by the application and specific to the product must be taken into consideration in the design, see tables.

                                                            Even in the case of actuators with track roller guidance systems, the load carrying capacity of the track roller guidance systems cannot be used to its full extent. In addition, the full static load carrying capacity of the track rollers cannot be supported, since the bolts in the track roller undergo deformation due to load.

                                                            Minimum load safety factor S0

                                                            Type of actuator

                                                            Precondition

                                                            Minimum load safety factor

                                                            S0

                                                            Linear actuators and linear tables

                                                            Predominantly oscillating load with stationary guidance system

                                                            20

                                                            All load parameters are known,

                                                            a linear unit supports the useful load at both ends,

                                                            deflection < 0,1% of the support distance

                                                            8

                                                            Linear actuators with track roller guidance system and linear tables LTE and LTS

                                                            Not all load parameters are known,

                                                            heavy contamination influence,

                                                            a linear unit supports the useful load over its complete surface,

                                                            milled, flat screw mounting surfaces

                                                            12

                                                            All load parameters are known,

                                                            no particular contamination,

                                                            a linear unit supports the useful load over its complete surface,

                                                            milled, flat screw mounting surfaces

                                                            6

                                                            Actuators with monorail guidance systems

                                                            Not all load parameters are known,

                                                            heavy contamination influence,

                                                            a linear unit supports the useful load over its complete surface,

                                                            milled, flat screw mounting surfaces

                                                            12

                                                            All load parameters are known,

                                                            smooth, vibration-free running,

                                                            no particular contamination,

                                                            a linear unit supports the useful load over its complete surface,

                                                            milled, flat screw mounting surfaces

                                                            4

                                                            Linear tables LTP and LTPG

                                                            Not all load parameters are known,

                                                            heavy contamination influence,

                                                            a linear unit supports the useful load over its complete surface,

                                                            milled, flat screw mounting surfaces

                                                            12

                                                            All load parameters are known,

                                                            smooth, vibration-free running, a linear unit supports the useful load over its complete surface,

                                                            no particular contamination,

                                                            milled, flat screw mounting surfaces

                                                            4

                                                            Minimum load safety factor S0 for overhead suspended arrangement

                                                            Type
                                                            of actuator

                                                            Precondition**

                                                            Minimum load safety factor

                                                            S0

                                                            Linear actuators and linear tables

                                                            Not all load parameters are known,

                                                            overhead suspended arrangement,

                                                            fewer than 2 linear units support a coherent mass

                                                            20

                                                            Not all load parameters are known,

                                                            overhead suspended arrangement,

                                                            at least 2 linear units support a coherent mass

                                                            or

                                                            all load parameters are known,

                                                            overhead suspended arrangement,

                                                            fewer than 2 linear units support a coherent mass

                                                            8

                                                            to

                                                            12

                                                            All load parameters are known,

                                                            overhead suspended arrangement,

                                                            at least 2 linear units support a coherent mass

                                                            6

                                                            to

                                                            8

                                                            **In the case of an overhead suspended arrangement, a drop guard is recommended.

                                                            © Schaeffler Austria GmbH